CodeWarrior for Microcontrollers v10.6 Update 1.0.0- simulator support for 56800EX digital signal controllers (DSC)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for Microcontrollers v10.6 Update 1.0.0- simulator support for 56800EX digital signal controllers (DSC)

1,303 Views
EngHuiPeng
NXP Employee
NXP Employee

How to get the 'chipview' pane to work where you can alter input values on pins or see output values. Is this support in this release?

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,096 Views
TICS_Fiona
NXP Employee
NXP Employee

Dear Hui Peng


Thanks a lot for contacting us.

56800EX simulator does not support hardware simulation like HCS08’s P&E Full Chip Simulation. 56800EX simulator can only simulate the Core instructions.

Hope it helps! If not, please reply me again. I will be very glad to help you.

Best Regards

Fiona

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply