CodeWarrior for MPC5xx v8.7 Install Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for MPC5xx v8.7 Install Issue

2,537件の閲覧回数
r40459
NXP Employee
NXP Employee

Hi

I'm having issues installing CodeWarrior for MPC5xx v8.7, failed to install windriver's kernel, is this a known issue?

 

Chris

ラベル(1)
0 件の賞賛
返信
1 返信

1,026件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Chris

On my computer, WinDriver is installed in:

C:\WINDOWS\System32\Drivers\windrvr6.sys

What's OS on your system?  CodeWarrior for MPC5xx V8.7 is not working on Win 7. It is a 32-bit application. Please view the note on its webpage:

CodeWarrior Development Tools for MPC5xx |NXP

It's not possible to install it under Win 7.

The installer stops when windrvr6.inf is installed.

For this installer is not possible to un-select this driver for the installation. We recommend using Windows 2000, Windows XP/Vista (32-bit). These are the official OS supported.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信