CodeWarrior for HC(S)08 and Windows Vista

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for HC(S)08 and Windows Vista

ソリューションへジャンプ
3,305件の閲覧回数
SergioSerna
Contributor I
Hi, the CodeWarrior special edition version 5.1 for HC (s) 08 does not install to me in Windows Vista. It is a this problem of my equipment or is of compatibility of software? Exists solution for the mutual incompatibility?
 
Thanks...
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
This is possible.
The HC08 V5.1 was not tested on Vista.
This version was released before Vista was available.
We support Microsoft® Windows® 98 SE/2000/XP
 
Please refer to the
Section System Requirements
 
The next version should support Vista.
However we can not give you any date.
 
Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,929件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
This is possible.
The HC08 V5.1 was not tested on Vista.
This version was released before Vista was available.
We support Microsoft® Windows® 98 SE/2000/XP
 
Please refer to the
Section System Requirements
 
The next version should support Vista.
However we can not give you any date.
 
Pascal
0 件の賞賛
返信