CodeWarrior for HC(S)08 & Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior for HC(S)08 & Linux

跳至解决方案
6,759 次查看
yurichi
Contributor I
Hi,
I'm working with Freescale NCB and SRB 13213 developing applications on beestack with beekit & Codewarrior special edition for HC(S)08. Is there a way to do this type of work using Linux (Ubuntu)? Codewarrior special edition for HC(S)08 for linux exists?
Tanks
标签 (1)
标记 (1)
1 解答
3,995 次查看
CrasyCat
Specialist III
Hello
 
We do not have Linux Hosted version of CodeWarrior for HC08.
We only provide Windows hosted development tool chain for that processor.
 
CrasyCat

在原帖中查看解决方案

6 回复数
3,995 次查看
bobbyAIR
Contributor I
Unfortunetly CW doesn't work under wine. I'v tried it but it failed
0 项奖励
回复
3,995 次查看
Navidad
Contributor III

I am well aware this is a very old thread, but anyway. The recently released CW for MCU works natively on Linux systems. It can be downloaded here.

0 项奖励
回复
3,995 次查看
bobbyAIR
Contributor I
But in my opinion, You should make CodeWarior multiplatform tool. There are many people who work under linux and just switch to Windows to work with Freescale uC's.
0 项奖励
回复
3,995 次查看
Navidad
Contributor III
yurichi, I don't know if this is a real solution for you, but you can use the build tools (and the debugger too) with wine under Linux.
0 项奖励
回复
3,996 次查看
CrasyCat
Specialist III
Hello
 
We do not have Linux Hosted version of CodeWarrior for HC08.
We only provide Windows hosted development tool chain for that processor.
 
CrasyCat
3,995 次查看
Nouchi
Senior Contributor II
Hi,

I don't what can it do, but you can have a look to the SDCC compiler (Small Device C Compiler) and works with many platforms (Win9x/NT/2000/XP Linux & Mac OS X) .
SDCC is Free Open Source Software, distributed under GNU General Public License (GPL).
I don't if there's support for S08 core.


Emmanuel
0 项奖励
回复