CodeWarrior for HC(S)08 & Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for HC(S)08 & Linux

Jump to solution
6,693 Views
yurichi
Contributor I
Hi,
I'm working with Freescale NCB and SRB 13213 developing applications on beestack with beekit & Codewarrior special edition for HC(S)08. Is there a way to do this type of work using Linux (Ubuntu)? Codewarrior special edition for HC(S)08 for linux exists?
Tanks
Labels (1)
Tags (1)
1 Solution
3,929 Views
CrasyCat
Specialist III
Hello
 
We do not have Linux Hosted version of CodeWarrior for HC08.
We only provide Windows hosted development tool chain for that processor.
 
CrasyCat

View solution in original post

6 Replies
3,929 Views
bobbyAIR
Contributor I
Unfortunetly CW doesn't work under wine. I'v tried it but it failed
0 Kudos
Reply
3,929 Views
Navidad
Contributor III

I am well aware this is a very old thread, but anyway. The recently released CW for MCU works natively on Linux systems. It can be downloaded here.

0 Kudos
Reply
3,929 Views
bobbyAIR
Contributor I
But in my opinion, You should make CodeWarior multiplatform tool. There are many people who work under linux and just switch to Windows to work with Freescale uC's.
0 Kudos
Reply
3,929 Views
Navidad
Contributor III
yurichi, I don't know if this is a real solution for you, but you can use the build tools (and the debugger too) with wine under Linux.
0 Kudos
Reply
3,930 Views
CrasyCat
Specialist III
Hello
 
We do not have Linux Hosted version of CodeWarrior for HC08.
We only provide Windows hosted development tool chain for that processor.
 
CrasyCat
3,929 Views
Nouchi
Senior Contributor II
Hi,

I don't what can it do, but you can have a look to the SDCC compiler (Small Device C Compiler) and works with many platforms (Win9x/NT/2000/XP Linux & Mac OS X) .
SDCC is Free Open Source Software, distributed under GNU General Public License (GPL).
I don't if there's support for S08 core.


Emmanuel
0 Kudos
Reply