CodeWarrior error - make:*** [projectname.obj] Error 5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior error - make:*** [projectname.obj] Error 5

ソリューションへジャンプ
2,001件の閲覧回数
Jonax7
Contributor I

Hi freescale community members! I´m a newcomer in freescale MCUs and in CodeWarrior software. My problem appear when I clean any project. I attached two pictures showing my problem.

 

The problem:

https://lh6.googleusercontent.com/--k_uOZH2RWU/UaTKC8HIQpI/AAAAAAAAAUI/eo_sLF_zAuA/w1278-h759-no/err...

https://lh5.googleusercontent.com/-Kbs0q8_BWfA/UaTKC0Hd3MI/AAAAAAAAAUE/qTsRUlgJ_fs/w1278-h759-no/err...

 

CodeWarrior version: 10.1 (Eclipse)

Freescale MCU: MC9S08JM32

Programmer: P&E Multilink

Language I tried to program: absolute assembly

Operative system: Windows 7

 

I hope you can help me. Regards!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,833件の閲覧回数
Rick_Li
NXP Employee
NXP Employee


Hi Jonax7,

I would recommend using the latest CW v10.4 which is available at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,834件の閲覧回数
Rick_Li
NXP Employee
NXP Employee


Hi Jonax7,

I would recommend using the latest CW v10.4 which is available at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

0 件の賞賛
返信