CodeWarrior error - make:*** [projectname.obj] Error 5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior error - make:*** [projectname.obj] Error 5

跳至解决方案
2,044 次查看
Jonax7
Contributor I

Hi freescale community members! I´m a newcomer in freescale MCUs and in CodeWarrior software. My problem appear when I clean any project. I attached two pictures showing my problem.

 

The problem:

https://lh6.googleusercontent.com/--k_uOZH2RWU/UaTKC8HIQpI/AAAAAAAAAUI/eo_sLF_zAuA/w1278-h759-no/err...

https://lh5.googleusercontent.com/-Kbs0q8_BWfA/UaTKC0Hd3MI/AAAAAAAAAUE/qTsRUlgJ_fs/w1278-h759-no/err...

 

CodeWarrior version: 10.1 (Eclipse)

Freescale MCU: MC9S08JM32

Programmer: P&E Multilink

Language I tried to program: absolute assembly

Operative system: Windows 7

 

I hope you can help me. Regards!

标签 (1)
0 项奖励
回复
1 解答
1,876 次查看
Rick_Li
NXP Employee
NXP Employee


Hi Jonax7,

I would recommend using the latest CW v10.4 which is available at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,877 次查看
Rick_Li
NXP Employee
NXP Employee


Hi Jonax7,

I would recommend using the latest CW v10.4 which is available at:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

0 项奖励
回复