CodeWarrior as a simple ICE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior as a simple ICE?

ソリューションへジャンプ
1,719件の閲覧回数
stephenhanka
Contributor I

I have never used CodeWarrior but I have a need for it.  I have CodeWarrior 10.1.1 targeting a P2040 running Linux with a USB JTAG TAP installed.  The board is occasionally locks up under certain conditions.  What I want to do is boot the board from flash wait for it to lock up, then break in with CodeWarrior and dump the registers, most importantly the program counter.

 

I don't see anything in the user documentation on how to do this.  I don't need to develop and download code.  I only want to dump the registers when the board locks up.  Can someone tell me if there is a simple way to do this?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,616件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have not used a P2040 with Linux, but I think this article might help you:

http://mcuoneclipse.com/2012/10/10/attach-connect-download/

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,617件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have not used a P2040 with Linux, but I think this article might help you:

http://mcuoneclipse.com/2012/10/10/attach-connect-download/

0 件の賞賛
返信