CodeWarrior and Windows 7 Home Premium (32 bit) crashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior and Windows 7 Home Premium (32 bit) crashing

ソリューションへジャンプ
3,678件の閲覧回数
offgrid
Contributor III

I've upgraded to Win 7 recently and I am finding CW very unstable. It locks up or unexpectedly quits after only a few minutes or seconds. I've tried all the compatibility mode tests, not much help there. My CodeWarrior version is V6.2, the IDE.exe ver is 5.9.0 build 2830. The pc is an HP laptop with all Win 7 updates.

 

It seemed to helped a little to change CW to Vista compatability and checking the box "Disable desktop composition" on the compatability tab of Codewarrior IDE properties. Also helping was removing the check in the box "Run as Administrator" for the entire CW folder.

 

But basically it will stay working for a minute or an hour, but typically will need to be shut down, or will shut itself down about 10 times a day!! It really does not like to have CTL-F pressed when being used within a second LCD monitor.

 

My question is, am I the only one, and if not what are others doing? Is version 10 supposed to be compatable with Windows 7, even though the specs say it's only working with Vista??!

 

Thanks

Tim

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,877件の閲覧回数
J2MEJediMaster
Specialist I

You need to file a service request on this. To do so, click here.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,878件の閲覧回数
J2MEJediMaster
Specialist I

You need to file a service request on this. To do so, click here.

 

---Tom

0 件の賞賛
返信
1,877件の閲覧回数
offgrid
Contributor III

The service request system is good, it's been a big help to me...but it is a little weird communicating with someone who can only reply once per day. The solution can often take days...if there is one.

 

I'm trying on Ver 10 for size..it's very own specs don't include the Windows 7 platform (which seems worrysome right?), but it on the other hand does seem more stable so far. It seems like an overkill solution for me ...it's very different than all the older versions of CW, but hey...I need a solution now.

 

Thanks, but for now...no thanks!!

 

Tim

Offgrid Engineering

0 件の賞賛
返信