CodeWarrior and FlexRay application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior and FlexRay application

3,037 次查看
pierrel
Contributor III

Hi,

I have tow FlexRay Evaluation Board from ON-semiconductors (NCV73810V2GEVB) which use the MC9S12XF512MLM microcontroller. I've planned to work with Code Warrior V.5.1. for programming it. I will work on FlexRay application. I don't have selected any Suite yet.

I was looking in the attached document which detail the differences between CW Suites and I wondered if the following restriction (or others that I did not see) could be anoying for FlexRay application :

  • C compiler and C source-level debugger–code and data size restricted to 32 KB (or 64KB for Basic suite),
  • C compiler and C source-level debugger for Freescale’s XGATE module (code and data size restricted to 512 KB).

 

Thanks.

标签 (1)
0 项奖励
回复
3 回复数

2,870 次查看
pierrel
Contributor III

Thank you Alice.

I have now an other question about CW suite. In theProfessional Suite, there is something about OSEK kernel awareness.

Can you tell me more about it ? Is it usefull or even essential for a FlexRay application ? I'm a novice in communication network.

0 项奖励
回复

2,870 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

In order to distinguish between different question , please create

another question about your new question , then we will continue

support it at the new thread , thank for your support .

BR

Alice

0 项奖励
回复

2,870 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

After you build your project , you can check the real code size on the .map file ,

then select the suite CW  license for you .

If still have any question or i misunderstand you , you can tell me without any

hesitate .

BR

Alice