CodeWarrior USP TAP ONCE connection failure.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior USP TAP ONCE connection failure.

1,597件の閲覧回数
yongcheolshin
Contributor II

I am working with HVP-56F82748 at CW MCU v11.0 and try to run example project "PMSM_Sensorless_FOC"

which is provided by freescale.

After building this project, I tried to invoke run, but it shows error below.

I am using CodeWarrior USP TAP ONCE as debugger.

pastedImage_1.png

But when I create a bareboard project, build, debug, there is no connection errors with USB TAP.

I can't understand.

Please help me..

0 件の賞賛
返信
1 返信

1,406件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yongcheol shin

Please compare the debug configuration on CW,

whether there is defference.

BR

Alice

0 件の賞賛
返信