CodeWarrior USP TAP ONCE connection failure.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior USP TAP ONCE connection failure.

1,598 Views
yongcheolshin
Contributor II

I am working with HVP-56F82748 at CW MCU v11.0 and try to run example project "PMSM_Sensorless_FOC"

which is provided by freescale.

After building this project, I tried to invoke run, but it shows error below.

I am using CodeWarrior USP TAP ONCE as debugger.

pastedImage_1.png

But when I create a bareboard project, build, debug, there is no connection errors with USB TAP.

I can't understand.

Please help me..

0 Kudos
Reply
1 Reply

1,407 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yongcheol shin

Please compare the debug configuration on CW,

whether there is defference.

BR

Alice

0 Kudos
Reply