CodeWarrior TRK Project Recompiling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior TRK Project Recompiling

Jump to solution
3,705 Views
rameshchandraka
Contributor III

Dear All

I have ported MPC5200b with new kernel.i want to use TRK application for my linux development with Code warrior GUI

I want recomile the TRK project ( code warrior project ) pointing towards latest kernel header and shared library.

compilation throwing lot of error

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,440 Views
Pavel
NXP Employee
NXP Employee

It looks like that AppTRK is used.

Look at the Section Modifying AppTRK of the "CodeWarrior TRK Reference.pdf" file.

This file is available in the attachment.

View solution in original post

0 Kudos
Reply
3 Replies
3,441 Views
Pavel
NXP Employee
NXP Employee

It looks like that AppTRK is used.

Look at the Section Modifying AppTRK of the "CodeWarrior TRK Reference.pdf" file.

This file is available in the attachment.

0 Kudos
Reply
3,440 Views
rameshchandraka
Contributor III

Dear Pavel

    I have already compiled this project with Code warrior IDE( Professional license).it is giving lot of error .some errors are related to pointers assignment.I have corrected that Errors. Now it is ending in Link error.Error Attached with this reply.Code warrior TRK Reference.pdf  ( Mobile GT processor) is referred for this issues.I have still touch with Freescale Support for Solving this issue.Errors attached -Message Window .

But if this issue is solved, linux App development is a enjoyable ...

--Regards

Ramesh

0 Kudos
Reply
3,440 Views
Pavel
NXP Employee
NXP Employee

Send please your project.

0 Kudos
Reply