CodeWarrior Starting Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Starting Problem

ソリューションへジャンプ
1,812件の閲覧回数
utsavikalpesh
Contributor V

Hi,

I download CodeWarrior v10.7 Offline for Windows . I install it and when I open it the following error is coming(Snap attached).

CodeWarriorStartError.png

Problem signature:
Problem Event Name: APPCRASH
Application Name: cwide.exe
Application Version: 0.0.0.0
Application Timestamp: 513dc971
Fault Module Name: cwide.exe
Fault Module Version: 0.0.0.0
Fault Module Timestamp: 513dc971
Exception Code: c0000005
Exception Offset: 0000d118
OS Version: 6.1.7600.2.0.0.256.1
Locale ID: 2057
Additional Information 1: 0a9e
Additional Information 2: 0a9e372d3b4ad19135b953a78882e789
Additional Information 3: 0a9e
Additional Information 4: 0a9e372d3b4ad19135b953a78882e789

Read our privacy statement online:
http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

If the online privacy statement is not available, please read our privacy statement offline:
C:\Windows\system32\en-US\erofflps.txt

How can I open codewarrior? Is it required any .dll or any settings? 

My system is of 32 bit.

Regards

Utsavi Bharuchwala

0 件の賞賛
返信
1 解決策
1,688件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- Please start CW IDE as admin option.

- There is host operating system support :

pastedImage_1.png

-There is a same problem with yours, you  can check it :

cwide.exe has  stopped working 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,689件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- Please start CW IDE as admin option.

- There is host operating system support :

pastedImage_1.png

-There is a same problem with yours, you  can check it :

cwide.exe has  stopped working 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,688件の閲覧回数
utsavikalpesh
Contributor V

Hi Alice_Yang,

Thanks for quick reply. Yes my codewarrior is now working ok just by run exe as admin.

Regards

Utsavi Bharuchwala

0 件の賞賛
返信