CodeWarrior Not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior Not working

跳至解决方案
2,323 次查看
McGillMike
Contributor I
I recently receved a BeeKit with 2 SRB boards and 1 NRB. When using CodeWarrior HC(S)08 V.5.1 to load applications, I get completely illogical behaviour: whenever i press on the "open" icon (or the menu option), or "import project" (or many others), CodeWarrior simply shuts down as if i had pressed on close or exit. I get no warning or error messages. I downloaded and installed all the updates. I tried removing and reinstalling the application. Nothing.
 
can anyone help me with this? 
 
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,587 次查看
CompilerGuru
NXP Employee
NXP Employee
This sounds like the bug described in this thread:
http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747

If this is this bug, there is also a workaround. I still wonder why I do not have this problem, it works fine for me.

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,588 次查看
CompilerGuru
NXP Employee
NXP Employee
This sounds like the bug described in this thread:
http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747

If this is this bug, there is also a workaround. I still wonder why I do not have this problem, it works fine for me.

Daniel
0 项奖励
回复