CodeWarrior Installation Qorivva error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Installation Qorivva error

3,284 Views
seoyeon
Contributor I

Hi,

I'm downloading CodeWarrior Development Studio for Microcontrollers v11.1, but QORIVVA is not installed properly.

The installation was not successful. Section will be skipped.
If the error persists, please contact Freescale Technical Support.

This message appears during installation and appears after installation is complete

QORIVVA - Error

There wasn't any log about this.

Previously, I've downloaded other codewarriers and I'm not sure if this is a problem. I deleted them before installing.

Thank you

0 Kudos
Reply
2 Replies

3,132 Views
stanish
NXP Employee
NXP Employee

Hello,

Have you downloaded the online or offline installer?

stanish_0-1751012122784.png

Offline installer does not need internet connection to install the MCU family packages.

I'd recommend you to download and install offline installer.

If both installers are causing an issue, please try to follow the steps below:

1)  uninstall/delete your previous versions of CodeWarrior you are not going to use any more.

2) reboot your computer

3) run the offline installer with administrator rights

4) choose Qorivva support in modular installer to be installed with CodeWarrior only and let other installer options default

Do you observe the same error again?

thanks for the update...

Stan

  

0 Kudos
Reply

3,154 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for delay. What's your target MCU? If it is not MPC560xB/C/D you can ignore the error message. 

0 Kudos
Reply