CodeWarrior HC16Z1 IDE - Forever Lost?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior HC16Z1 IDE - Forever Lost?

3,624件の閲覧回数
DavidH
Contributor I
I am looking for a copy of the CodeWarrior HC16Z1 IDE.  I have contacted the support people at Freescale but it seems their archive copy is corrupt.  Does anyone have a copy of the install .exe for this product?  Thank you.
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,892件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
What is exact product name you are looking for?

When I remember right, the last releases supporting the HC16 have been part of a combined installer for multiple processors (HC08, HC11, HC12, HC16,...).

Daniel
0 件の賞賛
返信

1,892件の閲覧回数
DavidH
Contributor I
Daniel,
 
Sorry, I do not have a model or release number.  The following Freescale webpage is all the info I can find.  My copy is corrupt and will not install.  Freescale's archive seems to be corrupt also.  If you have any info on models, releases or combined releases it may help me track down an image with Freescale.
 
 
Best regards,
 
David
0 件の賞賛
返信

1,892件の閲覧回数
CrasyCat
Specialist III
Hello
 
I do not have a web installer for CodeWarrior HC16, but I have an image of CD installer that I could zip and upload on a FTP site.
 
Would that help?
 
CrasyCat
0 件の賞賛
返信

1,892件の閲覧回数
PadelisGR
Contributor III

Hi there!

 

Sorry to bring this up again but is there an FTP that i could get that image file?

I want to write some code for a 68hc16 processor and i need it!

 

Thank you in advance

0 件の賞賛
返信