CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2 does not have option for the device 68HC912B32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2 does not have option for the device 68HC912B32

ソリューションへジャンプ
3,795件の閲覧回数
shivanandabairy
Contributor I

Hi,

I have downloaded and installed the 

CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2

It says that it supports the device 

but after opening the IDE, in the new project option I couldn't find the above device in the list.

 

If the above device is not supported in the v5.2, please tell me which version I can use for the above device.

ラベル(1)
タグ(2)
1 解決策
3,527件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW5.2 only supports limited HCS12(x) device,

This release includes support for the following derivatives:
    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
    - MC9S12G128, MC9S12G96
    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
    - MC9S12GN16, MC9S12GN32
    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
    - MC9S12XEP100, MC9S12XEP768
    - MC9S12XEQ384, MC9S12XEQ512
    - MC9S12XET256
    - MC9S12XS128, MC9S12XS256, MC9S12XS64
    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

-----------------------------------------

68HC912B32 is not on the list so CW5.2 doesn't support this device.

to work with 68HC912B32,  we use CW5.1 instead, attached is how to download CW5.1.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,528件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW5.2 only supports limited HCS12(x) device,

This release includes support for the following derivatives:
    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
    - MC9S12G128, MC9S12G96
    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
    - MC9S12GN16, MC9S12GN32
    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
    - MC9S12XEP100, MC9S12XEP768
    - MC9S12XEQ384, MC9S12XEQ512
    - MC9S12XET256
    - MC9S12XS128, MC9S12XS256, MC9S12XS64
    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

-----------------------------------------

68HC912B32 is not on the list so CW5.2 doesn't support this device.

to work with 68HC912B32,  we use CW5.1 instead, attached is how to download CW5.1.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,527件の閲覧回数
shivanandabairy
Contributor I

Hi Zhang,

Thanks for the reply,

I will try with CW v5.1

-Shivananda Bairy

0 件の賞賛
返信