CodeWarrior Debugger - Unable to download completing to the board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Debugger - Unable to download completing to the board

861 次查看
joonsinchu
Contributor II

Hi all,

 

I had connected all pins of the flatband cable to the BDM port of my board, hence the yellow LED and blue LED on the USB Multilink has turn ON.

 

Currently, I am using the chip processor of MC9RS08KB12, CodeWarrior 10.6.4 and USB Multilink interface to debug my code.

 

But, I am facing a problem on the debugging loading time. It keep showing "Downloading 312 bytes (99%)....." without completing it. Its take up the times much more longer than the usual debugging.

 

148753_148753.JPGerror6.JPG

148778_148778.PNGerror5.PNG

 

Does anyone encounter this situation before ? Anyone has any experience on this which can share to me ?

 

Hope to hear from you guys soon. Your feedback is much appreciated.

Thank you.

标签 (1)
0 项奖励
回复
1 回复

731 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

first we need identify the problem in hardware side, CW side, or specific project side.

can you please test:

1. create a new workspace

2. create a new project with wizard in this new workspace,

3. test if you can download the project to target without problem?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复