CodeWarrior 8- & 16-bit tools: printf() IN HC08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 8- & 16-bit tools: printf() IN HC08

3,193 Views
marc_paquette
Contributor V
To help you find solutions to problems that have already been solved, we have posted this message. It contains an entire topic ported from a separate forum. The original message and all replies are in this single message.
 
Posted: Jul 19, 2004 - 10:22 PM   
 
Hi there,
 
I'm using CodeWarrior 3.0 to compile my project for use on a MC68HC908JK1. When trying to debug my program, which does compile, I am inserting the printf() function and now my project won't compile.
 
Link Error: L1822: Symbol TERMIO_PutChar in file ...\ansii.lib is undefined
 
Could someone help me out by telling me how to get the printf to work.
 
Dean
Posted: Jul 20, 2004 - 04:44 PM   
 
Hi,
Just add the file termio.c from installation directory lib\HC12c\src to the project.
 
Ron
_________________
Ron Liechty
Ombudsman for Metrowerks
Posted: Jul 20, 2004 - 08:54 PM   
 
Hi Ron,
 
Thanks for tip but it opened up more problems,
now I am out of allocation space in segment ROM
 
I have stripped down all of my code trying to get this printf() function to work but there is still not enough room.
 
The ROM locations and size are:
 
$F600–$FBFF; user memory, 1536 bytes on MC68H(R)C08JK1.
 
Posted: Jul 20, 2004 - 10:02 PM   
 
As a follow-up to my last reply I am using a MC68HC08JL3 chip now for the sake of debugging. I plan to revert back to the JK1 once this is said and done.
 
So now there is enough ROM to compile but the True-time Simulator and Real-time Debugger is telling me I am using "invalid or unitialized memory" when I start my simulation
 
So now I've got two questions:
 
how to get printf() to compile onto a JK1?
 
AND
 
how do I get printf() to print to console (my screen)?
 
Posted: Jul 22, 2004 - 04:57 PM   
 
ANSI printf() take a lot ROM space. If your mcu is ROM limited
or use free SE CW HC08. Then you may code your won SCI utility like SendChar() / GetChar() / SendString()..
 
Check Compiler manual on how to generate compact code and
Manual_Engine_HC08.PDF -- P&E target interface for how to use full-chip-simulation properly.
 
mw_jcheng
Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies