CodeWarrior 4.5 for HCS12:long variables in printf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 4.5 for HCS12:long variables in printf

ソリューションへジャンプ
2,643件の閲覧回数
eddie
Contributor I
Using CodeWarrior 4.5 for HCS12(MC9S12NE64).
Does printf support long 32 bit variables?Don't seem
to be able to make it work.Any help would be appreciated.
Eddie
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,746件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
yes, it does support it, but make sure you have enough stack space defined.
Also consider that printf is both large in flash and in stack usage, using something more specifically tuned for your purpose may safe memory, but if space (RAM/FLASH) is not an issue, (s)printf does work for longs.

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,747件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
yes, it does support it, but make sure you have enough stack space defined.
Also consider that printf is both large in flash and in stack usage, using something more specifically tuned for your purpose may safe memory, but if space (RAM/FLASH) is not an issue, (s)printf does work for longs.

Daniel
0 件の賞賛
返信