Code generation bug?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,007件の閲覧回数
Oliver
Contributor III

I am having weird problems with CW4.7 for HC12. I am compiling some code from an older project, and I think the compiler may be generating the wrong code. Here's a snippet along with what the compiler generates (well, at least what the debugger assembly window shows):

 

// get a pointer from a const array, (p is allocated to Y)

p = ArrayAddresses[n];                // clra; asld; tfr d,x; ldy 37083,X

 

// copy value pointed to into some static variable

temp0 = *p;                              // ldd 0,y; std 0x0907

 

// now, here is the problem as I see it...

*pRam = *p;                             // ldd 2,y+; ldx 5,sp; std 0,x, sty 0,sp

p++;

 

 

The compiler generates "ldd 2,y+", which is the correct postincrement, but it should access 0,y instead of 2,y shouldn't it? Or am I missing something? I thought ldd 2,y+ loads D with the word pointed to by y+2, and then increments y. The target is a B32 derivative, if that makes any difference.

 

The postincrement seems to be throwing the compiler off, because if I drop the final p++, it generates:

 

*pRam = *p                               // ldd 0,y; ldx 5,sp; std 0,x

 

In general, I am having problems with code in the form *ptr++. I haven't tried switching any optimisations off yet, I wanted to check if this is a known problem.

 

Best regards,

 

Oliver

 

Message Edited by Oliver on 2009-03-09 12:39 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,346件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

> ldd 2,y+

Loads 0,y and then increments y by 2 (Post increment)

> ldd 2,+y

Increments y by 2 and then load D the location y points too after the increment (pre increment).

 

So the HC12 instruction set supports both, if the + is after the register, the register is post incremented and the access is at the previous register value. If the + is before the register, the register is preincremented and the location the new register value refers is accessed.

 

See "3.8.5 Auto Pre/Post Decrement/Increment Indexed Addressing" in the CPU12 reference manual.

 

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,347件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

> ldd 2,y+

Loads 0,y and then increments y by 2 (Post increment)

> ldd 2,+y

Increments y by 2 and then load D the location y points too after the increment (pre increment).

 

So the HC12 instruction set supports both, if the + is after the register, the register is post incremented and the access is at the previous register value. If the + is before the register, the register is preincremented and the location the new register value refers is accessed.

 

See "3.8.5 Auto Pre/Post Decrement/Increment Indexed Addressing" in the CPU12 reference manual.

 

Daniel

0 件の賞賛
返信