Code Warrior for MC9S12XF512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Warrior for MC9S12XF512

跳至解决方案
2,576 次查看
pierrel
Contributor III

Hi,

I have a FlexRay Evaluation Board from ON-semiconductors (NCV73810V2GEVB) which use the MC9S12XF512MLM microcontroller.

My question is : which CodeWarrior suite and version are able to program this microcontroller ?

I know that CodeWarrior Professionnal (V5.1) can help me because I have downloaded the eval version but there is anything about the Standard version.

 

Thanks

标签 (1)
1 解答
2,321 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

No matter the Special , the Basic , the Standard or the Professional CW5.1,

all can program this microcontroller .

The different is they have some different limitation , for example the data size.

The detail difference please check the "Quick reference guide for CW suites" in the

attachment .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,321 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Pierre

In addition to Alice’s answer, if you only need the feature of flash programming,  does not need to compile and debug the project, the Special Edition is OK, which is free.

http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

2,322 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

No matter the Special , the Basic , the Standard or the Professional CW5.1,

all can program this microcontroller .

The different is they have some different limitation , for example the data size.

The detail difference please check the "Quick reference guide for CW suites" in the

attachment .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------