Code Warrior True-Time Simulator & Debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Warrior True-Time Simulator & Debugger

跳至解决方案
3,591 次查看
CaptMike2452
Contributor I
I am using Code Warrior which came with the DEMO9S08AW60E Evaluation Board.

When I load an S19 file into the debugger, a dialog appears which says:
"Load Image contains flash memory data", "Erase and program flash?"

I  click "YES" and  the  CPROGHCS08 Programmer window appears.

The program automatically executes;  CM, EM, and PM, however, when the PM (Program Module) is executed,  I get the following error message:

"Programming and verifying address  $01860 Error during programming."
"Error 18 during script"

In other posts I have read a suggestion to use the "Expert Mode Programmer"

When I use the Expert Mode Programmer, and perform Erase Module, and Program Module, I get no error.

Question:

Why at this level of maturity for this product does the Erase and Program function  within the True-Time Simulator and Debugger not work?

Thanks,
Mike



标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,495 次查看
Alban
Senior Contributor II
Hello Mike,

Unfortunately you forgot to read the   [IMPORTANT] When Asking about CODEWARRIOR !!!

There is a crucial point missing: the version you are using + which cable ?!
Please come back with it.

The product you use has been tested and is supposed to work.
I don't see any product that is recognizing the S08AW60 and would not program it, that is a basic S08 product in term of programming and is supported.

The language you use let me thinh you are using the USB Multilink from P&E Microcomputers + their associated "third party" software add-on to CodeWarrior. But the rest is doesn't come to my crystal ball :smileywink:

Cheers,
Alban.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,496 次查看
Alban
Senior Contributor II
Hello Mike,

Unfortunately you forgot to read the   [IMPORTANT] When Asking about CODEWARRIOR !!!

There is a crucial point missing: the version you are using + which cable ?!
Please come back with it.

The product you use has been tested and is supposed to work.
I don't see any product that is recognizing the S08AW60 and would not program it, that is a basic S08 product in term of programming and is supported.

The language you use let me thinh you are using the USB Multilink from P&E Microcomputers + their associated "third party" software add-on to CodeWarrior. But the rest is doesn't come to my crystal ball :smileywink:

Cheers,
Alban.
0 项奖励
回复