Code Warrior Project - The directory name is invalid error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior Project - The directory name is invalid error

2,199 Views
donikuy
Contributor III

Hi,

 

I am trying to build the eGUI project using Code warrior and I get the errors below:

107833_107833.pngpastedImage_0.png

 

Any idea why this would happen?

 

 

Kind Regards,

Ylber Doniku

Labels (1)
0 Kudos
Reply
3 Replies

1,962 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Yiber,

Does the error gives more details about which directory is invalid? Could you attach the project so I can test it on my side?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply

1,962 Views
donikuy
Contributor III

Sorry I gave up on that project. Now trying to run another egui and get a lot of errors, which i think originate from the library paths. If you look at the picture below the libraries have a warning sign. Why do you think is that? I am assuming that stops my project building. I am using CW10.6 and MQX 4.1.

pastedImage_0.png

Thanks,

Ylber

0 Kudos
Reply

1,962 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Yiber,

I don't think that is what is causing the errors, the warning sign seems to be shown because the Libraries paths are relative paths. Could you post a screenshot of the errors you get? Maybe the compiler include paths are the ones that are incorrect?

pastedImage_0.png

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply