Code Warrior Eclipse IDE Closes Itself

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior Eclipse IDE Closes Itself

ソリューションへジャンプ
2,444件の閲覧回数
ahmetonur
Contributor I

Hello,

 

There is a .tlc file is passed from system promt by batch file like below,

 

# tcl script to download and execute

 

# start debug session using current active debug configuration

debug;

 

# wait for one second

wait 1000;

 

# remove all breakpoints

bp all off;

 

# set breakpoint at the end of execution

bp exit;

 

# start execution

go;

 

# remove all breakpoints

bp all off;

 

# terminate the debug session

kill;

 

# finally exit the IDE

quitIDE;

 

Code Waririor IDE closes itself when debug command is seen on debugger shell.

 

Could you please help me about the problem.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,238件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

This problem has been logged under the SR# 1-2645015401.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,238件の閲覧回数
ahmetonur
Contributor I

Hi,

I could not see your message about solution of the problem when I looked the service request section.

I see only "Request Researched and Reassigned".

0 件の賞賛
返信
2,238件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I contacted Jennie who is the owner of the SR.

She will provide you update next week (located in ASIA).


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,239件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

This problem has been logged under the SR# 1-2645015401.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信