Code Warrior 10.2 in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior 10.2 in Linux

3,336 Views
edasanli
Contributor I

Hi, I am using CodeWarrior 10.2 in Linux 16.04. I want to programming my S08PT60 EVK with using PE Micro Multilink Universal. But I have some problems in Debug and Flash Programmer section. Code Warrior can see my Multilink but this screen comes one after another. Does anyone give me a solution? Have a nice day.

Labels (1)
0 Kudos
Reply
3 Replies

3,251 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Eda,

Your IDE has detected P&E probe but can't connect.

This problem may be on either PC or board. We need identify it first.

Please test your board connection on another windows computer. Can''t it be connected as well? 

Create a new project in a new workspace, can it be connected?

Jun Zhang

0 Kudos
Reply

3,251 Views
edasanli
Contributor I

Hi, thanks for your advice.

I created new project and re-tested, still have this problem. Also I already tried on Windows computer with Code Warrior 11.1 it works on Windows. 

By the way, I used S08PT60-EVK board embedded debug interface. It worked on Linux. But I wonder why PEMicro doens't work.

I have a little question, can I program MC9S08PA4 on CodeWarrior 10.2? I need to use Linux.

0 Kudos
Reply

3,251 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes,  CW10.2 support PA4.

I suggest you provide your linux version to P&E to check if they have separated driver for this.

0 Kudos
Reply