Classic CW 6.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Classic CW 6.3

2,315 Views
zhouzhuoqiang
Contributor I

Hi. Zhang,

 

I installed Classic CW 6.3 in 32bit Windows XP, and try to flash s19 file to MC9S08AC60.

The step is: Hi-wave---->File---->Open configuration---->E2006_touch.ini, at this moment an error occurred.

The detail is " An  error occurred when executing command file: E2006_touch.hwl".

Here I attach our project files and I copied the error information from Hi-wave window in command area.

 

Could you kindly help me solve it?

 

Thanks!

Original Attachment has been moved to: E2006touch-project-files.zip

Labels (1)
0 Kudos
Reply
1 Reply

2,133 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please try if attached  E2006_touch.hwl can work for you?

just backup your old one and replace it with attached new file.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply