Classic CW 6.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Classic CW 6.3

2,306件の閲覧回数
zhouzhuoqiang
Contributor I

Hi. Zhang,

 

I installed Classic CW 6.3 in 32bit Windows XP, and try to flash s19 file to MC9S08AC60.

The step is: Hi-wave---->File---->Open configuration---->E2006_touch.ini, at this moment an error occurred.

The detail is " An  error occurred when executing command file: E2006_touch.hwl".

Here I attach our project files and I copied the error information from Hi-wave window in command area.

 

Could you kindly help me solve it?

 

Thanks!

Original Attachment has been moved to: E2006touch-project-files.zip

ラベル(1)
0 件の賞賛
返信
1 返信

2,124件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please try if attached  E2006_touch.hwl can work for you?

just backup your old one and replace it with attached new file.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信