Changing processor for a CW10.4 project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing processor for a CW10.4 project?

ソリューションへジャンプ
2,197件の閲覧回数
frankvanhooft
Contributor III

Apologies for the newbie question. Using CW10.4 under Windows I've imported the project for AN4370 (USB bootloader for the K20) and it's building fine. I need to actually target the KL25 processor. I understand I need to change the linker file. But how do I change the target processor? I see in the project properties it's saying Cortex-M4, but where can I change it to Cortex-M0?  (And is there anything else I should be doing?)

 

Thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,059件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

in CW10.2 and other past version, there is MCU Change Wizard. however CW10.3 and CW10.4 doesn't have MCU Change Wizard. It was removed. Because: - it only worked for simple cases - Customers tried unsuccessfully to use this wizard to change the target connection. This was NOT the intended purpose. our recommendation is to create a new CW MCU v10.4 project and drag ‘n drop files into the project

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,060件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

in CW10.2 and other past version, there is MCU Change Wizard. however CW10.3 and CW10.4 doesn't have MCU Change Wizard. It was removed. Because: - it only worked for simple cases - Customers tried unsuccessfully to use this wizard to change the target connection. This was NOT the intended purpose. our recommendation is to create a new CW MCU v10.4 project and drag ‘n drop files into the project

0 件の賞賛
返信
2,059件の閲覧回数
frankvanhooft
Contributor III

Thanks for the response. I might not be too excited about the answer (more work for me), but I'm impressed by the fast response. Thanks very much.

0 件の賞賛
返信
2,059件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!

0 件の賞賛
返信