Can't create a subproject

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't create a subproject

4,225 Views
robertpalmer
Contributor I
I have created a bunch of small projects for each of my plugins that I'm developing. I then created a new project using one of the templates. This new project is to be the "build all plugins" project.
I deleted everything from the template based project and attempted to add one of my plugin projects as a subproject. I tried by drag-n-drop and I tried by "Add Files..."

Neither worked. Both would bring up the dialog - "Which targets do you want to add to" but no files would get added.

Any ideas what I might be doing wrong?

IDE version 5.7.0 Build 1932
for Freescale HC12 4.5, build 6037
Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,673 Views
CrasyCat
Specialist III

Hello

I am working very often with sub-projects.

Normally you define a sub project dragging a .mcp file from explorer into CodeWarrior  current .mcp directory.

This is working fine for me.

It probably depends on what you did when you " deleted everything from the template based project ".

I would suggest you to submit a service request around that through our on-line support web page.

CrasyCat

0 Kudos
Reply

2,673 Views
robertpalmer
Contributor I
After much digging and still waiting on a response from sales, I discovered that:

1. I have the Special Edition
2. Not only does the Special Edition have a 32 file limit, it also has a restriction of NO SUB-PROJECTS. (It's buried in the descriptions in the Buyer's Guide document - not listed in any feature tables though).

Now I'm trying to figure out how far up I need to upgrade to get Sub-project functionality.
0 Kudos
Reply

2,673 Views
CrasyCat
Specialist III

Hello

If you are using HC08 Special Edition, 32K C Upgrade for Special Edition is enough.

If you are using HC12 special edition 64K C Upgrade for Special Edition is enough.

Please refer to the Buyers Guide on the corresponding CodeWarrior product page for more details.

For HC12 look at Buyers guide at http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272694011135

For HC08 look at the buyers guide at http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272694011860

I hope this helps.

CrasyCat

0 Kudos
Reply

2,673 Views
robertpalmer
Contributor I
From page 11 of the HCS12 document:

The C compiler upgrade to the full 64Kbytes offers:
- C compiler object code increased to up to 64Kbytes (1K of C++)
- No file limitation for the IDE
The C compiler upgrade offers:
- Unlimited C compiler (1K of C++)
- No file limitation for the IDE

Does "No file limitation for the IDE" also mean that sub-projects are allowed? This is not clear because in the limitations, you specifically list two items: #1) 32 file limit and #2) no sub-projects. In the upgrade, you only list a change to item #1.

Also, the above quote seems to imply that there are TWO upgrades - one that has a 64k C limit and one that has no C code limit. However, the table on page 10 only lists ONE upgrade. Am I reading something wrong?
0 Kudos
Reply

2,673 Views
CrasyCat
Specialist III

Hello

When the Buyers guide tells "No file limitation for the IDE" that removes both the 32 files per project limitation and the no sub-projects limitations.

The table on page 10 shows that unlimited IDE comes with the 64K C compiler upgrade. So sub projects are already possible with that package.

The table on Page 10 does not speak about the C Compiler upgrade you are right. With that upgrade, you can develop banked C application (application with more than 64K of code).

I will report to marketing that the buyers guide is not clear enough and that C compiler update is missing in the table.

CrasyCat

0 Kudos
Reply