Can Code Warrior not display extern memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can Code Warrior not display extern memory

ソリューションへジャンプ
2,245件の閲覧回数
terrybiberdorf
Contributor II

Hi have a TWR-K70F120M tower system.

 

I'm able to enable the DDR memory on the K70 board and run memory tests on it to verifies all read/write operations.

But when I attempt to view the memory (0x80000000+) with Code Warrior (CW10.4) I'm shown ???????? for each word.

 

Is there not a way to instruct CW10.4 to support view/modifying DDR memory directly?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,123件の閲覧回数
terrybiberdorf
Contributor II

Fix found.

I had to edit the MK70FN1M0.mem file found in my <project>/Project_Settings/Debugger/MK70FN1M0.mem

//     0x42000000 0x43FFFFFF         // Aliased to AIPS and GPIOC bitband

reserved   0x44000000 0x7FFFFFFF

range  0x80000000 0xDFFFFFFF 4 ReadWrite // 2GB DDR memory
//     0xE0000000 0xE00FFFFF         // Private Peripherals

reserved   0xE0100000 0xFFFFFFFF

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,124件の閲覧回数
terrybiberdorf
Contributor II

Fix found.

I had to edit the MK70FN1M0.mem file found in my <project>/Project_Settings/Debugger/MK70FN1M0.mem

//     0x42000000 0x43FFFFFF         // Aliased to AIPS and GPIOC bitband

reserved   0x44000000 0x7FFFFFFF

range  0x80000000 0xDFFFFFFF 4 ReadWrite // 2GB DDR memory
//     0xE0000000 0xE00FFFFF         // Private Peripherals

reserved   0xE0100000 0xFFFFFFFF

0 件の賞賛
返信
2,123件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

the DDR2 memory range is from 0x70000000 to 0x77FFFFFF on TWR-K70F120M, there is no memory after address 0x80000000.

0 件の賞賛
返信