CW5.1 PBMCUSLK  - code for function generator capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW5.1 PBMCUSLK  - code for function generator capture

2,369件の閲覧回数
Roaa
Contributor I
I've PBMCUSLK project board and i need to get the input from function generator , so i need the code to write it in my project
coeworriar version 5.1

--
Alban Edit: subject too vague


Message Edited by Alban on 2007-07-22 06:49 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,618件の閲覧回数
CrasyCat
Specialist III
Hello
 
I do not understand what you are trying to do here.
Can you be more specific?
 
What are you trying to achieve here?
Which code generator are you using? What problem are you facing?
 
CrasyCat
0 件の賞賛
返信

1,618件の閲覧回数
Roaa
Contributor I
i said i want a code for inputing data from function generator not a code generator!
i want this code to apply it in a project supporteed point to point wireless application
 
 
0 件の賞賛
返信