CW5.1 PBMCUSLK  - code for function generator capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW5.1 PBMCUSLK  - code for function generator capture

2,301 Views
Roaa
Contributor I
I've PBMCUSLK project board and i need to get the input from function generator , so i need the code to write it in my project
coeworriar version 5.1

--
Alban Edit: subject too vague


Message Edited by Alban on 2007-07-22 06:49 PM
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,550 Views
CrasyCat
Specialist III
Hello
 
I do not understand what you are trying to do here.
Can you be more specific?
 
What are you trying to achieve here?
Which code generator are you using? What problem are you facing?
 
CrasyCat
0 Kudos
Reply

1,550 Views
Roaa
Contributor I
i said i want a code for inputing data from function generator not a code generator!
i want this code to apply it in a project supporteed point to point wireless application
 
 
0 Kudos
Reply