CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

跳至解决方案
11,015 次查看
trav
Contributor III
Ok then how about this error.

Error starting external debugger.  Process Error Code 87 (0x57)
The parameter is incorrect.

Is there a work around for this?

Travis

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.
From: http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=5253



Message Edited by Alban on 2007-09-11 04:24 PM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,945 次查看
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,945 次查看
CompilerGuru
NXP Employee
NXP Employee
That problem has been fixed in CW for MCU's 6.0 (HC08) but not in the last released version for the HC12 (4.6) yet :smileysad:.
The problem is "just" when it tries to launch the external debugger hiwave.exe from within the ide.
A possible workaround would be to start hiwave.exe externally, see the arguments in the ide how hiwave is called, or start hiwave via explorer, load the *.ini as configuration and flash the *.abs explicitely.

Daniel

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.



Message Edited by Alban on 2007-09-11 04:25 PM
3,945 次查看
admin
Specialist II
Hi,

is this problem fixed allready?

I can start my debugger once,...
Than when i try it again it gives me that error code...

Greets Pieter
0 项奖励
回复
3,946 次查看
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel
0 项奖励
回复