CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

Jump to solution
10,957 Views
trav
Contributor III
Ok then how about this error.

Error starting external debugger.  Process Error Code 87 (0x57)
The parameter is incorrect.

Is there a work around for this?

Travis

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.
From: http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=5253



Message Edited by Alban on 2007-09-11 04:24 PM
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,887 Views
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel

View solution in original post

0 Kudos
Reply
3 Replies
3,887 Views
CompilerGuru
NXP Employee
NXP Employee
That problem has been fixed in CW for MCU's 6.0 (HC08) but not in the last released version for the HC12 (4.6) yet :smileysad:.
The problem is "just" when it tries to launch the external debugger hiwave.exe from within the ide.
A possible workaround would be to start hiwave.exe externally, see the arguments in the ide how hiwave is called, or start hiwave via explorer, load the *.ini as configuration and flash the *.abs explicitely.

Daniel

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.



Message Edited by Alban on 2007-09-11 04:25 PM
3,887 Views
admin
Specialist II
Hi,

is this problem fixed allready?

I can start my debugger once,...
Than when i try it again it gives me that error code...

Greets Pieter
0 Kudos
Reply
3,888 Views
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel
0 Kudos
Reply