CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW4.6 - Error starting external debugger.  Process Error Code 87 (0x57)

ソリューションへジャンプ
11,004件の閲覧回数
trav
Contributor III
Ok then how about this error.

Error starting external debugger.  Process Error Code 87 (0x57)
The parameter is incorrect.

Is there a work around for this?

Travis

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.
From: http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=5253



Message Edited by Alban on 2007-09-11 04:24 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,934件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,934件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
That problem has been fixed in CW for MCU's 6.0 (HC08) but not in the last released version for the HC12 (4.6) yet :smileysad:.
The problem is "just" when it tries to launch the external debugger hiwave.exe from within the ide.
A possible workaround would be to start hiwave.exe externally, see the arguments in the ide how hiwave is called, or start hiwave via explorer, load the *.ini as configuration and flash the *.abs explicitely.

Daniel

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.



Message Edited by Alban on 2007-09-11 04:25 PM
3,934件の閲覧回数
admin
Specialist II
Hi,

is this problem fixed allready?

I can start my debugger once,...
Than when i try it again it gives me that error code...

Greets Pieter
0 件の賞賛
返信
3,935件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Try using 4.7.
I assume this version addresses it, however I don't have vista or 4.7, so I cannot verify.
But I'm pretty sure this issue is fixed in 4.7.

Daniel
0 件の賞賛
返信