CW10 disable interrupt during step

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10 disable interrupt during step

Jump to solution
4,376 Views
IlConte
Contributor IV

I have installed Eclipse CW version.

I seek the function that disables interrupts during debugging step, in the IDE CW version.
Can help me ?
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,974 Views
IlConte
Contributor IV

I had unzipped  the file and did not unterstud what to do with its content (jar file).
Now I managed to install but I get an error:


View solution in original post

0 Kudos
Reply
9 Replies
3,974 Views
BlackNight
NXP Employee
NXP Employee

Hello,

you need to install the latest update to the 10.1 (as this is not present in the base 10.1):

Then you find the setting in the 'Interrupts' debugger settings:

 

BK

0 Kudos
Reply
3,974 Views
IlConte
Contributor IV

I have the 10.1 version, but in the debug configuration I do not see the interrupt tag

0 Kudos
Reply
3,974 Views
BlackNight
NXP Employee
NXP Employee

You need at least the 1.0.1 update for the 10.1 release.

Available from

www.freescale.com/cwmcu10

there select the 'download tab'

and download/install

MCU 10.1 Update for Windows: Adds Kinetis K50 family support, Processor Expert support for Kinetis 144, 100, and 80 LQFP packages, and Kinetis example projects.
Size (K): 275127 Format: zip Rev #: 1.0.1 Modified: 8/15/2011

 

Then the option should show up.

 

BK

0 Kudos
Reply
3,974 Views
IlConte
Contributor IV

I have downloaded the MCU 10.1 Update for Windws but now I cannot able to upgrade it.

How can i update with Jar file ?

 

Thanks

0 Kudos
Reply
3,974 Views
BlackNight
NXP Employee
NXP Employee

Menu Help > Install New Software.

Then press 'Add' button.

Use the 'Archive...' button to browse for the zip file you have downloaded.

 

BK

 

0 Kudos
Reply
3,975 Views
IlConte
Contributor IV

I had unzipped  the file and did not unterstud what to do with its content (jar file).
Now I managed to install but I get an error:


0 Kudos
Reply
3,974 Views
BlackNight
NXP Employee
NXP Employee

I see that you have CW installed in C:\program files. If you are using Vista or Windows 7: make sure you run the update as administrator. Otherwise Windows might deny installation of files.

 

BK

0 Kudos
Reply
3,974 Views
IlConte
Contributor IV

OK, now I have installed in Administrator mode and the installation proceed.

Moreover I have a timeout error:

 

0 Kudos
Reply
3,974 Views
IlConte
Contributor IV

OK, now connection with server OK.

All installed and Interrupt tag displayed !! :smileyhappy:

 

Thanks for help

0 Kudos
Reply