CW10.6 doesn't work in Win10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.6 doesn't work in Win10

Jump to solution
1,145 Views
huaping
Contributor III

I use CW10.6 well in old windows 7 system, but now failed to connect the target board (MC56F84789VLL )through USB-TAP or U-multilink ? Can you help check how to do, it seems driver issue? BTW, I already uninstall CW10.6 and install it again!

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
964 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Huaping

The host platforms that supported by CodeWarrior v10.6.4 include:

  • Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)
  • Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)
  • Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

It does not support USBTAP connection on Windows 10.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
965 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Huaping

The host platforms that supported by CodeWarrior v10.6.4 include:

  • Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)
  • Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)
  • Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

It does not support USBTAP connection on Windows 10.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply