CW10.4 simple question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.4 simple question

ソリューションへジャンプ
930件の閲覧回数
Florijan
Contributor III

Hi,

 

I am using CodeWarrior tools for many years. When I moved to CW10.4 and generated new Barebore Project for Kinetis L series MCU, I cant find "main.c" file. So my question is simple: Do I have to make this file by my self and if the answer is yes, which files I have to include using #include statement. If you have an example it would be also helpful. I could search these answers in documentation etc. but I really don't have time.

 

Best regards,

Florijan

ラベル(1)
0 件の賞賛
返信
1 解決策
830件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi,

which microcontroller do you use? I use the KL25Z, and a main.c is created for me inside the 'Sources' folder.

There is just one thing: if you create a Processor Expert project, then the main() is inside the ProcessorExpert.c file.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
831件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi,

which microcontroller do you use? I use the KL25Z, and a main.c is created for me inside the 'Sources' folder.

There is just one thing: if you create a Processor Expert project, then the main() is inside the ProcessorExpert.c file.

I hope this helps,

Erich

0 件の賞賛
返信