CW10.4 got problem after install update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.4 got problem after install update

1,215件の閲覧回数
changfuzhao
Contributor III

CW10.4 got problem after install update, does anyone have this problem?

6334_6334.jpgCW10.4.jpg

ラベル(1)
1 返信

1,001件の閲覧回数
kecart
Contributor III

Any time I see a problem with a fresh install not running properly, my first thought is it could be a Windows permissions problems.  If you downloaded the install from the internet onto a Windows 7 machine, the default behavior is for Windows to set the properties of the exe file to Blocked.  If you do not edit the properties of the install file (CW_MCU_v10.4_SE_Offline.exe was mine) and unblock it before running it, it will look like it installed but will give you all kinds of errors.  Assuming you used the default folder, check the properties for C:\Freescale\CW MCU v10.4\eclipse\cwide.exe.  If the properties show the file is blocked, uninstall everything, unblock the install exe file and reinstall everything.  I hope this helps you.