Is there anyway to set the format of the data variables displayed in tootips (if that is even what it is called)? For variables that are on the stack, hovering over the variable shows the value in the tooltip but that is set to automatic right now, and I get some foreign character. I just want to see the hex value. I have searched all through the doc set forums and don't see how to do this. It was easy under cw6.3, rt click, pick the format. Now rt click yields a massive set of useless irrelavent options many of which are not installed or do not work.
I appoligize if this is not the correct forum, this is as close as I could find.
Thanks
Robert
解決済! 解決策の投稿を見る。
There are the CodeWarrior forums where you can ask this question. However, in the interest of giving you a reply, I'll answer here. I've experimented around with the tooltips and suggest you file an on-line service request on this. Click here to do that.
---Tom
There are the CodeWarrior forums where you can ask this question. However, in the interest of giving you a reply, I'll answer here. I've experimented around with the tooltips and suggest you file an on-line service request on this. Click here to do that.
---Tom