CW10.1 dll missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,768件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I'm using a Softec Indart One probe, it worked with CW10.0, but SofTec_BDC08.dll is no longer  provided by CW10.1.

Softec systems are no longer suported?

 

Emmanuel

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,951件の閲覧回数
Nouchi
Senior Contributor II

Hi,

 

Never mind, I extracted SoftTec DLL from CW10.0 package and  it works fine.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,951件の閲覧回数
Ruth
NXP Employee
NXP Employee

CodeWarrior for Microcontrollers v10.1 does NOT include support for the SoftTec target interfaces. Unfortunately, SMH, the company that acquired SoftTec, decided not to update their DLLs to work with Windows 64-bit systems and Linux systems. Since CW MCU v10.1 was going to be offered on all these host operating systems, the decision was made not to include the 32-bit only SoftTec DLLs.

0 件の賞賛
返信
1,952件の閲覧回数
Nouchi
Senior Contributor II

Hi,

 

Never mind, I extracted SoftTec DLL from CW10.0 package and  it works fine.

0 件の賞賛
返信
1,951件の閲覧回数
aressm
Contributor I

I have same problem.

Can you help me to find DLL and how I can install it?

0 件の賞賛
返信
1,951件の閲覧回数
Bartel
Contributor I

Hello out there !

 

Bought me a new laptop - unfortunatly I wasn´t aware of the now upcoming compatibility problems !@@@!

Is there a solution for using indart one with WIN7 64bit ?

 

Thanks in advance for any kind of help ...

 

Regards,

Bartel

0 件の賞賛
返信
1,951件の閲覧回数
BlackNight
NXP Employee
NXP Employee

SofTec has produced a 32bit version of their DLL and for Windows XP only. But the DLL works as well under Vista 32bit (not sure about Windows 7 32bit).

But as for 64bit Windows, you need to have 64bit drivers as well, there is no solution (afaik) for 64bit.

 

BK

0 件の賞賛
返信
1,951件の閲覧回数
RoLee
Contributor I

Sorry for digging this up. But is there a chance to get the SofTec inDART HCS08 working with CodeWarrior 10.1 or 10.2 on Windows XP 32bit?

If there is a way to do so i would appreciate a short guide/howto.

 

Regards

RoLee

 

 

0 件の賞賛
返信