CW08 V5.0 HC08 chipset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW08 V5.0 HC08 chipset

跳至解决方案
6,702 次查看
Jerry
Contributor I
Hi.  I'm still fairly new to using Codewarrior and I'm trying to use the "SetStopMode" function for the MC68HC908QY4 chip, but for some reason it's "greyed out".  I can't seem to activate this function and was wondering if there's anything special I need to set in order to be able to use this function.  Could it be the possibility that I'm currently using the Special Edition license and need to upgrade to Standard or Pro?  and if that's the case, then which version do I need?
 
Thanks :smileyhappy:
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,210 次查看
ProcessorExpert
Senior Contributor III

Hi,

To activation SetStopMode function it is necessary to enable STOP instruction. The "Clock settings - Low Power Mode settings - STOP instruction enabled" property should be set to "yes" value in CPU Inspector window - Properties page.

Regards, Processor Expert Support

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,210 次查看
Jerry
Contributor I
That's exactly what I was looking for.   Thanks!
 
:smileyvery-happy:
 
0 项奖励
回复
3,211 次查看
ProcessorExpert
Senior Contributor III

Hi,

To activation SetStopMode function it is necessary to enable STOP instruction. The "Clock settings - Low Power Mode settings - STOP instruction enabled" property should be set to "yes" value in CPU Inspector window - Properties page.

Regards, Processor Expert Support

0 项奖励
回复
3,209 次查看
Jerry
Contributor I
Thanks for the reply roco, however, I actually have the 908QY4 chip and I'm using the SofTec InDart board for programming purposes.  This is the reason why I chose the chip at the beginning of Processor Expert in Codewarrior.  I realize that there is only 1 type of Stop mode in the QY4, however I can't seem to set any parameters that would allow me to use the "SetStopMode" function.  That's what made me wonder if it was the version of software I was using.  Changing the chipset in software may solve my problems with setting Stop mode, however, as I am limited to using this particular chip, does not quite solve my problem either.  Do you have any other suggestions for this particular chip?
 
Thank you for taking the time to reply.
0 项奖励
回复
3,209 次查看
rocco
Senior Contributor II
Hi, Jerry:

The problem is that the MC68HC908QY4 only has a single stop-mode.

All of the HC08 family processors have one stop mode, but with many variations, depending on how configure the peripherals. On the other hand, the HCS08 family has three stop modes. If you choose an HCS08 chip in CW, the stop-mode option should un-grey.
0 项奖励
回复