CW v5.1 Windows 10 - PE Multilink Universal FX Rev. C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW v5.1 Windows 10 - PE Multilink Universal FX Rev. C

2,958 次查看
ecorini
Contributor I

Hi,
I'm trying to debug an old project for HC12 developed with CW v5.1 in a Windows 10 platform.
I've successfully installed the CW 5.1 ide in windows 10, but when i start debugger from the DE the PE Micro device is not recognized.
The firmware of the PE Micro device is updated and the driver are the latest installed from PEMicro site.
Is it possible to use "PE Multilink Universal FX Rev. C" with CW 5.1 in windows 10 in any way?

If instead of "PE Multilink Universal FX Rev. C" i use an older "PE Multilink Universal Rev. A" (the green one) i can debug successfully.

Thank you very much.

0 项奖励
回复
3 回复数

2,661 次查看
ecorini
Contributor I

Hi,
the chip is MC9S12HZ128

Here (PEMicro forum) a link to a patch that should resolve the problem:
http://www.pemicro.com/forums/forum.cfm?forum_id=8&forum_topic_id=6810#c19992

0 项奖励
回复

2,661 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

OK. thanks.

0 项奖励
回复

2,661 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Emanuele Corini

Officially CW5.1 doesn't support win10, what's your chip part number? I will check if there is other solutions.

Thanks,

Jun Zhang

0 项奖励
回复