CW v5.1 Windows 10 - PE Multilink Universal FX Rev. C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW v5.1 Windows 10 - PE Multilink Universal FX Rev. C

1,579 Views
ecorini
Contributor I

Hi,
I'm trying to debug an old project for HC12 developed with CW v5.1 in a Windows 10 platform.
I've successfully installed the CW 5.1 ide in windows 10, but when i start debugger from the DE the PE Micro device is not recognized.
The firmware of the PE Micro device is updated and the driver are the latest installed from PEMicro site.
Is it possible to use "PE Multilink Universal FX Rev. C" with CW 5.1 in windows 10 in any way?

If instead of "PE Multilink Universal FX Rev. C" i use an older "PE Multilink Universal Rev. A" (the green one) i can debug successfully.

Thank you very much.

0 Kudos
Reply
3 Replies

1,282 Views
ecorini
Contributor I

Hi,
the chip is MC9S12HZ128

Here (PEMicro forum) a link to a patch that should resolve the problem:
http://www.pemicro.com/forums/forum.cfm?forum_id=8&forum_topic_id=6810#c19992

0 Kudos
Reply

1,282 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

OK. thanks.

0 Kudos
Reply

1,282 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Emanuele Corini

Officially CW5.1 doesn't support win10, what's your chip part number? I will check if there is other solutions.

Thanks,

Jun Zhang

0 Kudos
Reply