CW V5.0 hiwave.exe hangs up while using HC08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW V5.0 hiwave.exe hangs up while using HC08

4,685 次查看
Jarek
Contributor I
Hello everyone,
I.m so frustrated  - I'm using CW V5.0 for developing my project for HC908GP32 chip. I would like to debug it with Full Chip Simulation, hovever IDE hangs up  displaying the msg - loading target.
I traced problem to hiwave.exe. Even if the simulator is used in is stand alone mode (double click on hiwave.exe), the problem occurs if HC08 processor is selected in Set Connection panel. However, for HCS08 processor everything works fine.
Do any one of you experienced this problem? Is is just my PC or is is problem with Special Edition of CW V5.0.
Any help appreciated. Thanks.
Jarek 
 
 
标签 (1)
标记 (1)
0 项奖励
回复
5 回复数

1,872 次查看
Jarek
Contributor I

Hi,

I contacted Freescale Tech Support. It was confirmed that I had a correct version (not corrupted) of all the files. The new copy was send to me (they were great).

It was still causing problems, but I knew that it wasn't a CW problem. I decided to do a clean reload of Windows XP Prof with formatting my HD. It solved the problem. I still don't know what was a direct source of my troubles, but I'm running CW Sim and Deb.

Jarek      

0 项奖励
回复

1,872 次查看
KrisRutecki
Contributor III
Hi,
I know nothing about CW5, and equally much about windows, but quiet a few things about 08s.
How exactly are you connected to your target? Is there a special adapter from your PC to the target header, or do you have a socket for the micro and plug in the emulator there, just like in the old days?
Have you managed to program your chip at least once?
0 项奖励
回复

1,872 次查看
Jarek
Contributor I

Hi Kris,

to answer you questions:

- yes, I managed to program the chip with my own programmer I build using P&E Micro sotware.

- with regard to CW - I just want to test the code with full chip simulation. To do this, you don't need a programmed chip. You would just select HC08 processor and Full Chip Simulation option on the connection panel of Real Time Simulator/Debagger program (hiwave.exe).

Regards, Jarek    

0 项奖励
回复

1,872 次查看
CrasyCat
Specialist III

Hello

Which OS are you running on your Host system (Windows 200, XP SP2, ...)?

Can you do the following:

 - Start IDE
 - Select Help -> "About Freescale CodeWarrior"
 - Click on Installed products.

What is written on the top portion of the dialog?

How did you activate the Full Chip simulator? Using the Change MCU/Connection dialog?

Can you send the file "HC08_Full_Chip_Simulator.ini" from your project directory?

CrasyCat

0 项奖励
回复

1,872 次查看
KrisRutecki
Contributor III
Ahemm,
Well then, can't help much here... I do everything on a Mac, you see, and then software µP emulators were never at the top of my list, either.
Good luck,
Kris
0 项奖励
回复