CW 6.0 Visualization Tool querry.??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 6.0 Visualization Tool querry.??

ソリューションへジャンプ
2,229件の閲覧回数
Destiny
Contributor I
Dear all
  
   Currently I am reading some values from the Microcontroller. So for easy to read option I am using the Visualisation tool
   In visualisation tool I am using the Value as text option, so the values which are displaced are rounded ones, but instead I would be glad to have values with digits after the decimal points.
   So is there any way to get complete value in Visualisation tools,  instead of rounding off ones???

thanks in advanced

Regards
Destiny
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,459件の閲覧回数
CrasyCat
Specialist III
Hello
 
The visualization tool is not able to display a floating point value.
 
It displays the hexadecimal encoding of the variable (or the decimal representation of the 4-byte value read as a long).
 
You may want to submit a feature request if you need to get that supported in the visualization tool.

Click here to submit a service request.

 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,460件の閲覧回数
CrasyCat
Specialist III
Hello
 
The visualization tool is not able to display a floating point value.
 
It displays the hexadecimal encoding of the variable (or the decimal representation of the 4-byte value read as a long).
 
You may want to submit a feature request if you need to get that supported in the visualization tool.

Click here to submit a service request.

 
CrasyCat
0 件の賞賛
返信