CRC Calculation In Linker

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CRC Calculation In Linker

3,892件の閲覧回数
tunayan
Contributor II

Dear Community members,

 

I have to find a way to calculate CRC of specific memory area in linker stage.

So I have developed a CAN bootloader and i want to compare the both CRCs before programming and run-time.

 

I am using MPC5644A Dev kit. And My IDE is CW 10.6

 

I tried to follow below  comments but, it is not proper with my mcu exactly.

CRC of Data section in Load Memory location

 

Thanks all.

ラベル(1)
2 返答(返信)

2,936件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I'm using the SRecord tool for CRC calculation, see CRC Checksum Generation with ‘SRecord’ Tools for GNU and Eclipse | MCU on Eclipse

I hope this  helps,

Erich

2,936件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Tuna

The Qorivva linker does not support this feature as DSC does.

But you can use the ‘crcgen.exe’ included in CodeWarrior v10.6.5 to generate a CRC in building.

For details, please see the section 5.1.7 in FAQ Guild:

C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF\MCU_Power-Architecture_Compiler.pdf

But this solution can only get CRC in building. In run-time, user needs to add his own code to get CRC in application project.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------