CAU_LDD unsupported in upgrade from 10.6 to 10.6.4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAU_LDD unsupported in upgrade from 10.6 to 10.6.4?

1,599件の閲覧回数
panometric
Contributor I

Importing a project from 10.6, but it will not build on 10.6.4 because Processor Expert will not generate code for the crypto module. The CPU is MCF51QM128VHS. The help for the module shows fine, and the files appear to be installed.

But the processor expert window says that CAU_LDD  module is not supported in this version of Processor Expert. See attached.  How can this be fixed? 

タグ(1)
0 件の賞賛
返信
1 返信

1,412件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

CAU_LDD component is deprecated and not integrated in the new version.

Our recommendation is

Crypto Acceleration Unit: CAU and mmCAU software library|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信